Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Whether it's called a surge, a sag, a spike, a transient, a fluctuation, an interruption, or noise, "dirty power" is some type of abnormality in the electricity that runs your facility.

Whether it's called a surge, a sag, a spike, a transient, a fluctuation, an interruption, or noise, "dirty power" is some type of abnormality in the electricity that runs your facility.

Dirty power originates outside of and within your facility. Sources like lightning, utility switching, capacitor switching, and faults on the utility's distribution system can all affect the quality of your power before they even reach your facility.

And daily fluctuations from internal electrical equipment—like devices that run in cycles or get turned on and off frequently—can cause cumulative and equally damaging power hazards. Even a small appliance can cause problems in sensitive equipment that share the same line. And the more electrical equipment a company uses, the more transients accumulate.

Here are some common power disturbances and how to detect them:

 

Power Disturbances  Definitions  Causes Possible Computer Symptoms
Normal Mode Noise(Amplitude 0.5V to 25V) Low-level signals, superimposed on the power sine wave Computers, switching power supplies, power line modulation equipment Processing errors, incorrect data transfer, terminal or printer errors
Normal Mode Impulses and Ringing Transients
(Amplitude 50V to 6kV)(Duration: 5 µsec to 2000 µsec)
A narrow, fast-rise voltage variation. Followed by a damped oscillation decaying to nominal in less than one cycle Switching loads on or off, computers, utility switching, lightning Incorrect data, processing errors, printer or terminal errors, hardware damage
Common Mode Disturbances(Amplitude: millivolts - hundreds of volts) Impulses and EMI/RFI noise superimposed on the power conductors Radios, computers, arcing contacts, lightning Incorrect data transfer, terminal or printer errors, I/O hardware damage
Sags
(Duration: Greater than one cycle)
A low-voltage condition on one or more phases Ground faults, starting large loads, low-power system capacity, lightning System crashes, hardware damage
Harmonics
(Duration: Less than one cycle)
Quick voltage variations, harmonics occur at the natural multiple of the standard power wave Switching nearby loads off/on, computer networks, utilities Data corruption, processing errors, incorrect data transfers, lock-ups, hardware damage
Overvoltages
(Duration: Greater than one cycle)
A high-voltage condition on one or more phases Rapid load reduction, utility switching Hardware damage
Outage
(Duration: Greater than half a cycle)
A zero-volt condition Ground faults equipment failure, accidents, lightning, acts of nature System crashes, hardware damage

Related Articles

Partner Login

Language & Location