Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv™ Liebert® PSI5 lithium-ion UPS models provide longer battery life and runtime and deliver lowest total cost of ownership

Columbus, Ohio [March 2, 2020] – Vertiv, a global provider of IT infrastructure and continuity solutions, today announced the availability of lithium-ion models of the Vertiv™ Liebert® PSI5 uninterruptible power supply (UPS) family. The Liebert PSI5 is the first single-phase UPS from Vertiv available with lithium-ion batteries. With their increased runtime and reduced maintenance requirements, lithium-ion batteries are a natural fit for deployments at the edge of the network, where IT support is limited. The Liebert PSI5 lithium-ion line interactive UPS is available now for customers in the U.S. and Canada, in 1500VA and 3000VA capacities.

The lithium-ion option eliminates the weakest link in the power chain at the edge, doubling the battery life and reducing total cost of ownership (TCO) by up to 50% compared to traditional valve-regulated lead acid (VRLA) batteries. The Liebert PSI5 leverages the superior energy density of lithium-ion batteries to enable significantly longer runtime in a similar footprint. It delivers up to 20 minutes of runtime at half load and 9 minutes at full load – roughly double that of similarly-sized UPS systems – and is well suited for small spaces in distributed networks. The Liebert PSI5 comes with a five-year advanced replacement warranty, contributing to a significantly lower TCO.

“More and more digital applications are being shifted to the edge of the network, where on-site IT support is limited, yet they are no less critical than most enterprise data centers and need the same level of power protection,” said Ramesh Menon, vice president and general manager of single phase UPS for Vertiv. “Lithium-ion batteries are a perfect choice for edge sites because they bring reliable, ‘set it and forget it’ performance with an attractive TCO. The Liebert PSI5 with lithium-ion batteries eliminates the frequent battery refreshes required with VRLA batteries and enables savings and stability for IT managers with edge facilities.”

The Liebert® PSI5 with lithium-ion batteries comes with a battery management system (BMS) that provides real-time monitoring of battery conditions and ensures safe and reliable operation.

“Vertiv already has a robust selection of single-phase UPS systems, but a lithium-ion unit is a great option to have when trying to help customers meet their needs, especially as they want longer battery life for less maintenance at the edge of their networks,” said David Walty, channel account manager for Data Power Technology, a Vertiv partner who assisted in the selection and deployment of Liebert PSI5 lithium-ion models for a local manufacturing facility.

Liebert PSI5 lithium-ion models will also be eligible for the recently announced Vertiv™ Trade-In Program. This program enables customers to trade in almost any aging single-phase UPS – Vertiv and competitive systems – for discounted pricing on new Vertiv Liebert PSI or Vertiv™ Liebert® GXT UPS systems. The Trade-In Program also includes free shipping and recycling of the surrendered UPS units, in compliance with the Recycling Industry Operating Standard (RIOS).

Vertiv made the announcement at CRN XChange in San Antonio. The Liebert PSI5 is available from Vertiv distributors, D&H, Ingram Micro, SYNNEX and Tech Data, and through the Vertiv channel.

For more information on the Liebert PSI5 with lithium-ion batteries or any data center solutions from Vertiv, visit Vertiv.com.
 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
 

CONTACT

Schuyler Easterling
T +314-982-8673
E Schuyler.Easterling@fleishman.com

Related Articles

Partner Login

Language & Location