Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Performance As Promised

Liebert Cooling Products Earn Trusted AHRI CERTIFIED® MARK

Vertiv, through its Liebert cooling systems, is the first and only data center and telecom cooling system provider based in the U.S. to have its products earn the AHRI Certified® mark from the Air-Conditioning, Heating, and Refrigeration Institute (AHRI) under its new Datacom 1360 program.

Download Brochure View Infographic

We Deliver As Promised



For years, people have relied on certifications from the Air-Conditioning, Heating, and Refrigeration Institute (AHRI) for air conditioning systems used in homes and businesses for non-critical applications.

Until now a customer was more likely to know how their 1-ton woodshop cooling unit would perform in capacity and efficiency, than they were about the 10- ton unit cooling their mission critical data center.

Without AHRI certification in the datacom industry, a data center or telecom customer had no way of knowing the actual capacity and efficiency of their cooling solution, unless they spent months and tens of thousands of dollars on independent testing. As a result, cooling is often over provisioned and over designed.

To address this issue, Vertiv, under its Liebert brand,  worked with AHRI to create a certification process for data center and telecom cooling equipment.

Now customers can be assured they are getting the capacity and efficiency they are promised, without the need to overprovision or perform expensive independent testing.

Read the Press Release

Talk to an Expert

Partner Login

Language & Location