Vertiv Geist Environmental Monitors
Environmental factors like heat, humidity and moisture pose a severe threat to mission-critical infrastructure. These dangers can be minimized by incorporating an environmental monitoring solution to collect data and alert users of potential threats. Vertiv Geist Environmental Monitors allow users to securely observe conditions and receive alerts when user defined thresholds are breached.
Dit product is op uw dashboard opgeslagen
U hebt dit product zojuist op uw dashboard opgeslagen om op een later tijdstip te bekijken. U kunt het item eenvoudig van uw dashboard verwijderen als u het niet langer wilt opslaan.
Meld u aan of maak een account aan om dit voor later op te slaan
- Bankwezen, financiën en verzekeringen
- Omroepwezen en Entertainment
- Datacenter/colocatie/hosting
- Onderwijs
- Overheid
- Gezondheidszorg
- Industrie
- Militair, defensie, luchtvaart en raketten
- Telecom
- Transport
- Detailhandel en groothandel
- Professionele services
Vertiv Geist Environmental Monitors
Environmental factors like heat, humidity and moisture pose a severe threat to mission-critical infrastructure. These dangers can be minimized by incorporating an environmental monitoring solution to collect data and alert users of potential threats. Vertiv Geist Environmental Monitors allow users to securely observe conditions and receive alerts when user defined thresholds are breached.
- Bankwezen, financiën en verzekeringen
- Omroepwezen en Entertainment
- Datacenter/colocatie/hosting
- Onderwijs
- Overheid
- Gezondheidszorg
- Industrie
- Militair, defensie, luchtvaart en raketten
- Telecom
- Transport
- Detailhandel en groothandel
- Professionele services
Specificaties
Vertiv Geist Environmental Monitors include on-board temperature, humidity, and dew point sensors. Additional Plug-n-Play and Dry Contact/ 0-5V sensor capacity enables users to deploy a comprehensive and cost-effective environmental monitoring solution to minimize risks to critical infrastructure.
Watchdog 100-UK
|
||
---|---|---|
Environmental Monitor | AC 100-240V, 50/60Hz | 2 Plug-n-Play and 4 Dry Contact / 0-5VDC |
Meer productinformatie bekijken |
Voordelen
Kenmerken
* Voor modelspecifieke downloads dient u naar de modelspecifieke productpagina te gaan door de naam van het model te selecteren in bovenstaande specificatietabel.
Vind de contactpersoon in uw regio
Contactpersonen productsupport
Wijzigen
Veelgestelde vragen
- V
- Why do I have an alarm showing tripped even though the current value is below the threshold?
- A
- Each alarm has a 1-unit hysteresis built-in to help limit nuisance alarms. This means that a value must change by 1 unit before the alarm will clear. For example, if there is a temperature alarm set with a high trip of 75F, the value must fall below 74F before the alarm will actually clear. A clear delay will need to be set and configured on the that alarm.
- V
- How can I re-order the sensor OIDs on a Watchdog device?
- A
- To change the order in which sensors are mapped to an OID the user will need to unplug all sensors from the device and wait 1-2 minutes until they show unplugged on the web interface (will read unavailable at first). After they show unplugged, check the "remove all unplugged devices" box and then click the save changes button. After a couple minutes they can begin reconnecting sensors in the order you would like them in.
- V
- My Watchdog 15 is showing a higher temperature than what my thermostat is showing.
- A
- In still air environments the onboard sensor is susceptible to higher temperature readings due to circuit board heating. With that, air temperatures in a room are rarely, if ever, uniform throughout the space, due to convection currents, relative proximity to sources of heat and cold air, and other thermal effects. Our Watchdog products have an internal temperature offset that you can adjust to compensate for board heating. This is found by selecting the Configuration Wrench in Sensors-Overview.